Scegli la tua regione e lingua

Vai

Menu

Rourkela-Raipur

Customer Story | 2 min read

TCSC for stable transmission of surplus power from Eastern to Western India

Power Grid Corporation of India Ltd (PGCIL) has purchased two Thyristor Controlled Series Capacitors (TCSC) from Hitachi Energy. The banks were installed on the Rourkela-Raipur double circuit 400 kV power transmission interconnector between the Eastern and Western regions of the grid. The length of the interconnector amounts to 412 km.

The main purpose of this major AC inter connector is to enable export of surplus energy from the Eastern to the Western regions of India during normal operating conditions, and also during contingencies. The TCSC are located at the Raipur end of the lines. The TCSC enable damping of interarea power oscillations between the regions, which would otherwise have constituted a limitation on power transfer over the interconnector. Dynamic simulations performed during the design stage, and subsequently confirmed at the commissioning and testing stage, have proved the effectiveness of the Raipur TCSC as power oscillation dampers. Furthermore, system studies performed showed no risk for Sub-Synchronous Resonance (SSR) in the Indian network.

Main data  
Parameter Fixed Segment TCSC Segment
Nominal system voltage 400 kV 400 kV
Rated line current 1550 A 1550 A
Line current overload, 30 minutes 2093 A 2093 A
Line current overload, 10 minutes 2325 A 2325 A
Physical capacitor reactance 54,7 Ω 6.83 Ω
Nominal capacitive boost factor 1.0 1.2
Boost factor range - 1.0-3.0
Rated capacitor reactive power 394 Mvar 71 Mvar
Rated capacitor bank voltage 84.8 kV 12.7 kV
Degree of compensation 40% 5% (@ 1.0 boost factor)
ZnO rating (incl. redundancy) 56 MJ 15 MJ
Power oscillation damping
TCSC reactance response