Scegli la tua regione e lingua

Vai

Menu

Scaling at the speed of AI: Supporting AirTrunk’s expansion across Singapore and Malaysia

Customer Story | 4 min read

The rapid adoption of AI and cloud technologies is reshaping digital infrastructure requirements, driving significant growth in data center capacity across the globe. As operators respond by developing larger, higher-density campuses, they must balance the need for expansion with the equally critical priorities of power reliability, operational resilience, and environmental performance.

To accommodate rapidly growing demand for cloud services and increasingly power-intensive AI workloads, AirTrunk, one of the Asia-Pacific region's leading hyperscale data center operators, is expanding its capacity across Singapore and Malaysia. These investments help ensure the scalable, reliable infrastructure needed to support the evolving requirements of hyperscale customers and the continued growth of the digital economy in the region.

The Challenge

Meeting growing capacity deamands in Asia

Expansion in Singapore

965538762

AirTrunk’s Singapore operations already provide more than 180MW of IT capacity, anchored by SGP1 in Loyang, the country's largest independent data center by megawatt capacity. Designed to support hyperscale cloud customers, SGP1 features diverse 66 kV power feeds, BCA Green Mark Platinum certification, and energy-efficient infrastructure that has set a high benchmark for performance and sustainability. 

As demand for cloud services continues to accelerate, AirTrunk is expanding its presence with SGP2, a new hyperscale facility expected to provide more than 70MW of additional capacity. 

Expansion in Malaysia

Medium wide shot of male IT professional looking at laptop while working on server in data center

In Malaysia, AirTrunk is developing JHB2, its second data center campus in Johor, designed to scale beyond 270MW of capacity. As a cloud and AI-ready facility, JHB2 represents a significant investment in supporting the region's rapidly growing digital economy and strengthening Johor's position as a major data center hub. 

The Solution

Supporting critical data center operations across two markets

To support both projects, AirTrunk worked with Hitachi Energy’s Transformers business to provide the critical power infrastructure. 

For SGP2, Hitachi Energy supplied two 100 MVA power transformers. Power transformers convert electricity from the grid to the voltage levels required by critical data center systems, including servers and cooling equipment, enabling power to be delivered efficiently, safely, and reliably. Designed to operate reliably under heavy loads, the transformers help support the uptime and resilience expected of hyperscale data centers. Together, they form a key part of the facility's power backbone, providing dependable power delivery as capacity requirements grow.

For JHB2, Hitachi Energy supplied three 275 kV, 100/80 MVA ester-filled power transformers. In data center environments, where uninterrupted operations are critical, even a single fire incident can threaten business continuity and lead to costly downtime. The ester-filled transformers help mitigate this by offering a biodegradable alternative to conventional mineral oil with a significantly higher fire point and lower flammability, enhancing the safety of the facility. This provides an additional layer of protection for critical power infrastructure while supporting AirTrunk's sustainability objectives.

The Impact

Creating a foundation for future capacity

With both projects underway, AirTrunk is positioned to continue growing across two of its key APJ markets. SGP2 extends a Singapore facility base that already delivers more than 180MW of certified, sustainable IT capacity. In Malaysia, JHB2's planned scalability beyond 270MW builds on the existing JHB1 facility, with the two sites expected to provide more than 420MW of capacity supporting cloud and AI services across the region.

Long before users stream content, train AI models, or access cloud applications, the underlying power infrastructure must already be in place. By supplying transformers for AirTrunk's developments in Singapore and Malaysia, Hitachi Energy is helping ensure that the capacity being built today is ready to support the digital demands of tomorrow and the next generation of data center development across Asia-Pacific.

In Data Center: Male IT Technician Running Maintenance Programme on a Laptop, Controls Operational Server Rack Optimal Functioning. Modern High-Tech Telecommunications Operational Super Computer.
Shot of Corridor in Working Data Center Full of Rack Servers and Supercomputers.

Explore transformer solutions for Data Center applications

Discover transformer solutions supporting reliable and scalable data center operations