Scegli la tua regione e lingua

Vai

Menu

Waratah Super Battery, Australia

Customer Story | 4 min read

Customer

Akaysha Energy is an Australian developer, owner, and operator of mega-scale battery energy storage systems (BESS). With over 40 GWh of storage in development globally, Akaysha is unlocking flexible, revenue-generating assets that accelerate the clean energy transition.

Chosen by the Government of New South Wales to deliver the Waratah Super Battery, one of the world's most powerful batteries, Akaysha Energy is helping strengthen grid reliability and support the State's ambitious goal of reducing CO2 emissions by 70% while building, owning and operating this landmark project. 

Project Details

Customer:

Akaysha Energy

Location:

New South Wales, Australia. Site of the decommissioned Munmorah coal-fired power station  

Capacity:

850 MW / 1,680 MWh BESS

Challenge

Deploy a grid-scale BESS capable of ultra-fast, automated response to external shocks while enabling long-term revenue through ancillary services trading

Solution

288 Power Conversion Systems (PCS)

Two Power Plant Controllers (PPC)

Engineering and integration services

Digital control systems

Multi-phase testing to validate grid compliance and fast-response performance

Web 2400x1028 - 5

Challenge

Push battery performance beyond standard limits to protect the grid and unlock new revenue

Developing and delivering the 850 MW / 1,680 MWh BESS Waratah Super Battery meant solving more than technical complexity. To qualify, Akaysha Energy had to meet some of the industry’s most demanding grid-code requirements and prove compatibility with the System Integrity Protection Scheme (SIPS), a fast-acting control system operated by Transgrid that detects grid disturbances and triggers automated battery response within milliseconds.

This meant integrating advanced control systems, validating performance through rigorous testing and modelling, and ensuring seamless operation under Australia’s most stringent regulatory standards.

At the same time, Akaysha structured the project to align with their broader business model of turning Waratah into a flexible, revenue-generating asset through participation in ancillary services markets.

Solution

To meet these challenges, Akaysha Energy partnered with Hitachi Energy to deploy a digitally enabled infrastructure stack that could respond to grid events within milliseconds while also meeting Australia’s regulatory standards. This integrated solution combines advanced power electronics, intelligent control systems, and real-time automation to deliver fast, compliant, and coordinated grid support.

At its core are Hitachi Energy's Power Plant Controllers (PPC) and Power Conversion Systems (PCS). Sitting behind the battery and the SIPS Control System developed by Transgrid are Hitachi Energy's smart controls and software, the digital brains behind the project. The entire solution was validated through a rigorous testing regime, ensuring reliable performance under real-world conditions and full compatibility with SIPS.

By combining engineering expertise, compliance support, scalable technology, and HMAX™ Energy, Hitachi Energy's AI-powered suite of services and solutions designed to safeguard critical energy systems, Hitachi Energy helped transform Waratah into a resilient, revenue-generating asset ready to support both grid stability and market participation. Through a 20-year service agreement, real-time monitoring, diagnostics and advanced analytics provide continuous visibility of system performance and lifecycle support, helping maximize asset availability, optimize long-term performance, and ensure the system continues delivering value throughout its operational life.

Reaching final commercial operations at the Waratah Super Battery is a significant milestone for everyone involved. The partnership between Akaysha Energy and Hitachi Energy has been instrumental in delivering one of Australia's most important energy infrastructure projects.

Nick Finch, Director of Engineering, Akaysha Energy

Hitachi Energy's best-in-class Power Conversion Solution
 

  • Efficiently integrate BESS into the grid
  • Form factor reduces installation costs
  • Multilevel coordinated control ensures fast dynamic response
  • Robust design for maximum power in extreme environments
  • Full power rating up to 1500 VDC ensures efficient project sizing

What 1,680 MWh Can Do:

Power 80000 Australian homes

for a full day

112 million phones

Charge every smartphone in Australia more than four times

Only 50000 Milliseconds

Required to respond to grid disturbances 

Impact

Command complexity. Power security.

The Waratah Super Battery is a foundational step in New South Wales’ energy transition, supporting the phase-out of coal-fired power stations, enabling greater integration of renewables, and helping the state move toward its goal of reducing emissions by 70% by 2035. While the system has only recently reached commercial operation, its potential to deliver fast, automated grid support is already clear. During a severe heatwave in November 2024, the Waratah Super Battery was called upon by the Australian Energy Market Operator (AEMO) to help maintain system reliability during a period of exceptionally high demand in New South Wales, providing an early demonstration of the value large-scale battery storage can deliver to the electricity system.

Command complexity. Power security. In practice, that means helping operators manage increasingly complex energy systems while ensuring critical infrastructure can adapt to evolving grid requirements and continue delivering reliable performance and long-term value.

As operations ramp up, Waratah is expected to play a growing role in stabilizing the grid, reducing carbon emissions, and unlocking new business models for clean energy deployment.

Waratah Super Battery   

1,680 MWh

ICON

70%


Australia’s* largest standby battery — and one of the world’s most powerful

*at time of commissioning

Strengthens grid reliability and resilience by responding to disturbances in milliseconds

Supports the state’s plan to cut emissions 70% by 2035 and reach net-zero by 2050

Power Conversion Solutions

Discover our innovative portfolio of digitally-enabled conversion and control solutions for connecting renewables and storage to the grid.