Scegli la tua regione e lingua

Vai

Menu

Workshop Repairs for Traction Transformers

As a crucial part of the traction chain, the onboard traction transformer adapts the electrical voltage from the overhead power lines to the lower voltage levels needed within the traction chain. It also feeds auxiliary converters for other electrical systems like lighting, heating, and/or onboard information systems.

If the traction transformer fails, the planned train traffic schedule may be disturbed and leads to passenger inconvenience, and even costly penalties may be incurred.

Workshop repairs for Traction Transformers

Scope of work

A traction transformer is highly reliable and designed to perform under harsh conditions. However, to prevent unpredicted failure and ensure a long lifetime, some services are advised during the whole life cycle.

The operating conditions of a traction transformer differ highly from power transformers. Therefore the interpretation of condition checks has to be done by traction experts; otherwise, misleading results may occur.

Regular oil analysis gives a good image of the actual health. Additionally, basic and advanced diagnostic tests can provide further information.

If an onboard traction transformer gets damaged by an accident or due to other reasons, we are able to fully repair the traction transformer by replacing damaged parts of the core, winding reclamping, partial or full winding replacement, and repair of the tank. At the end of such work, all electrical routine tests are done.

During the long lifetime of a vehicle, some operational conditions change. Upgrading or replacing some parts of the traction transformer can help ensure further operation.

A midlife overhaul is recommended to ensure reliability in the second half of the lifetime. All traction transformers are systematically checked and maintained by replacing parts with lower lifetime expectancy.

Workshop Repairs for Distribution and Small Power Transformers

Hitachi Energy offers workshop repairs for distribution and power transformers ranging from 315 kVA to 5 MVA.

Workshop Repairs for Medium and Large Power Transformers

Hitachi Energy offers workshop repairs for medium and large power transformers.

Transformer Refurbishment

Hitachi Energy offers refurbishment services to cover transformer rehabilitation and sustainable life extension to advance a sustainable energy future for all.

On-site Repairs

Hitachi Energy offers on-site repairs to bring the transformer factory setup to the work site with the TrafoSiteRepair™ service that is executed to the same high-quality standard as a workshop repair.

Transformer Component Upgrades

Transformers component upgrades are based on Hitachi Energy's decade-long experience in manufacturing and maintaining its products.

24/7/365

Our Global Service Teams are here to support you anytime!

Get to know more

Assistenza per trasformatori

Le risorse obsolete, l’aumento della domanda di energia e la necessità critica di evitare interruzioni impreviste stanno mettendo alla prova le aziende di servizi di pubblica utilità e gli industriali di tutto il mondo. Il portafoglio di servizi di Hitachi Energy consente alle aziende di servizi di pubblica utilità e agli industriali di massimizzare il ritorno sulle risorse dei trasformatori garantendo un’affidabilità elevata accompagnata da un abbassamento dei costi del ciclo di vita e garantendo prestazioni ottimizzate e la riduzione dell’impatto ambientale.
LYS186599_2

Trasformatori

Hitachi Energy offre trasformatori di distribuzione e di potenza, trasformatori di tipo a secco ed EconiQ™, nonché servizi per applicazioni industriali e commerciali.

Isolamento e componenti dei trasformatori

Il portafoglio più ampio e affidabile al mondo di componenti e sistemi di isolamento per trasformatori