Choose your region and language

Go

Menu

AxoniQ™ for multi-terminal DC

AxoniQ™

AxoniQ™ takes traditional HVDC systems to the next level, supporting efficient, reliable and scalable multi-terminal DC grids for the next step in asset and investment optimization.

What is MTDC?

MTDC stands for multi-terminal DC. While traditional HVDC systems are typically point to point connections, MTDC extends this concept into a DC Grid, where more than two terminals are connected. This allows power to be routed flexibly, delivering electricity where it’s needed and when it’s needed.

Key benefits

Reliable
Resilient
Affordable
Flexible

The new era of DC grids

As global electricity demand accelerates, MTDC systems are becoming critical to ensuring a secure, affordable, and sustainable power grid. As renewable energy deployment accelerates and power systems become increasingly interconnected, MTDC systems help manage congestion and improve resilience by allowing dynamic power flow between multiple terminals and across different energy markets, while supporting faster planning, procurement, and execution of grid projects. By connecting multiple power sources and demand points, MTDC grids enable electricity to be directed where it is needed most.
Shot of Corridor in Working Data Center Full of Rack Servers and Supercomputers.
Increasing demand on electricity
Alternative energy - Aerial view of offshore windmill park at sea.
Renewable energy deployment accelerates
Higher interconnectivity between regions

MTDC is gaining strong interest today among transmission system operators and developers because the need of the power systems are changing rapidly. The increasing integration of renewable generation and expansion of cross‑border power exchange are driving higher demands for controllability, flexibility, and resilience. 

What is AxoniQ™ portfolio?

Marking a significant step toward greater interoperability, the launch of AxoniQ comes as governments and grid operators worldwide accelerate investments in transmission infrastructure toward a fully electrified world to integrate renewable energy at scale, strengthen cross-border interconnections, and improve energy security. The AxoniQ portfolio combines advanced power electronics and control technologies. It includes:

DC AxoniQ™ Protect

An innovative solution that can interrupt a DC fault in less than three milliseconds, it offers fast and effective protection at up to 525 kilovolts (kV). It enables selective fault isolation by disconnecting only the affected section of the DC grid, while the rest of the system continues operating. This continuous, proactive protection enables extremely low losses and the optimal combination of performance, efficiency, and reliability throughout the entire lifecycle.   

DC AxoniQ™ Connect

A modular DC switching station that enables the connection of new terminals and structures the grid into several protection zones, creating manageable subsystems. AxoniQ Connect ensures reliable service continuity, simplifies maintenance, and supports cost-efficient scalability.

DC AxoniQ™ Control

An advanced control system built with interoperability in mind that maintains voltage stability and power balance, optimized power flow, and flexible, market-driven energy exchange. AxoniQ Control addresses congestion and enables quick reconfigurations in the event of disturbances. 

Listen to our experts

What is MTDC, and why does it matter right now for the future of power systems?

 

How can HVDC and MTDC strengthen reliability and resilience as electrification grows?

How does MTDC make the grid more flexible on a day-to-day basis?

How can MTDC help optimize infrastructure and reduce overall system costs?

Selected references

Part of categoryCustomer Story

SACOI3

Part of categoryCustomer Story

Saudi Arabi - Egypt

Part of categoryCustomer Story

Caithness Moray link

Part of categoryCustomer Story

Shetland

Part of categoryCustomer Story

Zhangbei

Part of categoryCustomer Story

Raigarh - Pugalur

Part of categoryCustomer Story

North East Agra

Part of categoryCustomer Story

Quebec - New England