Choose your region and language

Go

Menu

Hitachi Energy in Iraq

Hitachi Energy has supplied 120+ mobile substations and 30+ transmission substations in Iraq over 15 years.

120+ mobile substations, 30+ transmission substations, and the National Control Center since the 1970s

 

Hitachi Energy has a long-standing legacy in Iraq's power sector supplying over 120 mobile substations, delivering more than 30 transmission substations in the past 15 years, and continuously upgrading key assets like the National Control Center since its original installation in the 1970s, leveraging global technology and local expertise. 

Abbasid threshold in Karbala, Iraq

Locations Map

See all Hitachi Energy Locations in Saudi Arabia

Learn more about us

Explore more

FAQ

Yes. Hitachi Energy has a long-standing legacy in Iraq's power sector, combining global technology with local expertise.

Hitachi Energy has supplied over 120 mobile substations and delivered more than 30 transmission substations in Iraq over the past 15 years.

Hitachi Energy's relationship with Iraq's power sector dates back to the original installation of the National Control Center in the 1970s, which it has continued to upgrade since.

Hitachi Energy originally installed the National Control Center in the 1970s and has continuously upgraded the asset since.

Utilities and transmission, oil and gas, and public infrastructure sectors.

Enquiries can be made through the Hitachi Energy Middle East contact page, and Iraqi locations can be found via the locations map filtered to Iraq.

Contact us

Photo of
Ayman Ismaeil

Head of Communications & Government Relations - Middle East & Africa