Upgrading reliable sensor technology with a modern IEC 61850 process bus
Customer Story | 3 min read
Digital substations upgrading
Customer Story | 3 min read
Digital substations upgrading
The Australian electricity transmission company Powerlink Queensland owns and operates Queensland’s high voltage electricity transmission network. In this digital substation project, Hitachi Energy drew on its extensive experience with non-conventional instrument transformers (NCITs) to replace the originally installed proprietary process bus with IEC 61850 technology and connected the primary (high-voltage) equipment to the substation protection and control devices more effectively, improvig the reliability and availability of the optimized substations.
In 2011 the first commercial process bus installation, the so called digital substation, was successfully put into operation. This first digital substation outside of China was only the first of a series of six outdoor substations with process bus and NCIT technology. The second and the third substations were put in service in 2013 and 2014 respectively.
In this project, Powerlink Queensland makes use of the SAS600 station automation system from Hitachi Energy, Relion® 670 series protection and control IEDs and the REB500 distributed busbar and breaker failure protection system.
All protection and control equipment in the system are connected to the IEC 61850-9-2 process bus and receive analog sampled values from the CP-MU merging units also supplied by Hitachi Energy. New sensor electronics connect the MUs to the existing combined current and voltage sensors. This approach allowed the refurbishment of the primary technology to be kept to a minimum.
Thanks to the integrated redundancy of the NCITs from Hitachi Energy, two completely independent systems of merging units and protection equipment were implemented to meet the customer’s redundancy requirements.
The replacement of copper wires by fiber optic cables and the description of the transferred information according to IEC 61850 opened new opportunities for intelligent testing tools to support the commissioning and maintenance of the substation.
In addition to the described projects, Hitachi Energy installed several pilot installations to prove further products from Hitachi Energy‘s digital substation offering, like FOCS, the optical current transformer and to help customers gain experience with this technology.
The modernization of the installations with the latest technology in accordance to IEC 61850 supports Powerlink Queensland in its mission to responsibly deliver electricity transmission services that are valued by shareholders, consumers, customers and the market.
| Main data | |
|---|---|
| Device | Function |
| Process level | |
| ELK-CP | Non-conventional redundant instrument transformers for current and voltage measurement in gas-isolated switchgear |
| CP-MU | Non-conventional redundant instrument transformers for current and voltage measurement in gas-isolated switchgear |
| Bay level | |
| REC670 | Bay control IED |
| REL670 | Line distance protection IED |
| RED670 | Line differential protection IED |
| RET670 | Transformer differential protection IED |
| REB500 | Busbar and breaker failure protection system |
| Station level | |
| RTU560 | Communication gateway to control center |
| MicroSCADA Pro | Substation automation system |
| Auxiliary facilities | |
| Building | Transportable building for protection and control cabinets, automation system and auxiliary facilities |