Hitachi Energy’s pioneers HyFlex hydrogen-powered generator with shore power system for ships at berth

Press Release | Sweden | 07.05.2025 | 2 min read

  • The two-week test at the Majnabbe terminal for Stena Line’s Germany traffic demonstrated Hitachi Energy’s hydrogen-powered generator as a viable energy source for clean power in ports
  • HyFlex is an emission-free alternative to diesel generators, providing clean electricity for ships at berth
  • Collaboration with Stena Line, Power Cell Group, Linde Gas, and the Port of Gothenburg accelerates sustainable solutions for port operations

Gothenburg, May 7, 2025 - Hitachi Energy has successfully demonstrated HyFlex™, an innovative energy supply system based on zero-emission hydrogen-powered fuel cell technology, in collaboration with Stena Line, Power Cell Group, Linde Gas, and the Port of Gothenburg. In a two-week test, HyFlex generated electricity using green hydrogen as fuel while connected to the existing shore power system for ships on one of Stena Line’s ferry vessels.  

HyFlex is a cutting-edge, emission-free system that produces electricity, heat, and water. It is flexible, scalable, and designed as a portable plug-and-play unit, making it easy to transport and use immediately. This innovative solution effectively addresses challenges such as locally constrained grids or remote power needs. Compared to conventional diesel power generators running continuously, a 1 (megavolt-amperes) MVA HyFlex can mitigate up to 1,600 tons of diesel fuel per year, translating into 5,800 tons of CO2 saved.

The initiative at the Port of Gothenburg has taken a significant step forward by connecting HyFlex directly to the local power grid to demonstrate its grid-supporting capabilities. The valuable field data collected will enhance the solution that is currently under development, showcasing the potential of hydrogen as an energy carrier and the technical viability of fuel cell technology in port environments.

Importantly, this collaboration on hydrogen-powered generators has become particularly relevant in light of the new EU regulations in 2030, requiring ships over 5,000 gross tonnages to use an onshore power supply (OPS) or zero-emission technology in ports1.

“For Stena Line, it is natural to collaborate in testing new technology aimed at reducing emissions from our industry. This project demonstrates that there are alternative paths for ports lacking adequate infrastructure for electricity connection.”

Anders Peterson, Group Head of Port Development & Engineering at Stena Line

“We are delighted with the results of the most recent collaboration with Stena Line, Power Cell Group, Linde Gas, and the Port of Gothenburg. We appreciate working with these relevant industry players to continue exploring new application areas for HyFlex and demonstrate its broad potential, from construction sitesto ship terminals, to accelerate the energy transition.”

 Tobias Hansson, CountryManaging Director at Hitachi Energy in Sweden


This successful demonstration of HyFlex builds on Hitachi Energy’s previous innovative efforts, such as the project to decarbonize a construction site in the Port of Gothenburg. In that initiative, the islanded hydrogen-powered generator supplied clean power for an electric excavator, marking the first demonstration at a customer site. Furthermore, it shows the scalability and versatility of HyFlex in various applications, reinforcing its potential to drive sustainable energy solutions across different sectors. 

Footnote

1 Regulation (EU) 2023/1805 of the European Parliament and of the Council of 13 September 2023 on the use of renewable and low-carbon fuels in maritime transport, and amending Directive 2009/16/EC. https://eur-lex.europa.eu/eli/reg/2023/1805/oj/eng

About Hitachi Energy

Hitachi Energy is a global technology leader in electrification, powering a sustainable energy future with innovative power grid technologies with digital at the core. Over three billion people depend on our technologies to power their daily lives. With over a century in pioneering mission-critical technologies like high-voltage, transformers, automation, and power electronics, we are addressing the most urgent energy challenge of our time – balancing soaring electricity demand, while decarbonizing the power system. With an unparalleled installed base in over 140 countries, we co-create and build long-term partnerships across the utility, industry, transportation, data centers, and infrastructure sectors. Headquartered in Switzerland, we employ over 50,000 people in 60 countries and generate revenues of around $16 billion USD.

https://www.hitachienergy.com
https://www.linkedin.com/company/hitachienergy
https://x.com/HitachiEnergy


About Hitachi, Ltd.

Through its Social Innovation Business (SIB) that brings together IT, OT (Operational Technology) and products, Hitachi contributes to a harmonized society where the environment, wellbeing, and economic growth are in balance. Hitachi operates globally in four sectors – Digital Systems & Services, Energy, Mobility, and Connective Industries – and the Strategic SIB Business Unit for new growth businesses. With Lumada at its core, Hitachi generates value from integrating data, technology and domain knowledge to solve customer and social challenges. Revenues for FY2024 (ended March 31, 2025) totaled 9,783.3 billion yen, with 618 consolidated subsidiaries and approximately 280,000 employees worldwide. Visit us at https://www.hitachi.com.

Contact

Photo of
Charlotte Lindevall

Communication Manager Sweden

More information

All news