Choose your region and language

Go

Menu

Modular Advanced Control for HVDC (MACH™)

The control system is the brain in HVDC transmission systems. One of the most important advantages with modern HVDC technology is the controllability.

The Modular Advanced Control for HVDC (MACH™) control system provides unequalled calculation capacity and enables a high degree of integration and handling for all control and protection functions. Moreover,

Modular Advanced Control for HVDC (MACH™) control provides advanced fault registration and remote control functions. The system is designed to run 24/7 for thirty years or more, allowing the HVDC system to be controlled and protected in the most reliable way throughout its life time.

To fulfill current and future requirements Hitachi Energy has developed the Modular Advanced Control for HVDC (MACH™) system as a fully computerized one, using state-of-the-art computers, microcontrollers and digital signal processors connected by high-performance industrial standard buses and fiber optic communication links. Because of the extensive use of computers and micro-controllers, it has been possible to include very powerful internal supervision, which eliminates periodic maintenance of the control equipment.

The system consists of the station control and monitoring servers, operator workstations, control and protection main computers, digital signal processor units, I/O systems and valve control units. Thanks to the modularity and high performance of the MACH equipment, the type of hardware and system software used for a VSC-HVDC  control system are the same as in an LCC-HVDC or a FACTS control system. In fact, only the application software and the valve control differs.

The ability to upgrade is yet another advantage with Modular Advanced Control for HVDC (MACH™). That means even an older HVDC system can enjoy the benefits of great controllability. This is a great way to prolong the lifetime of an existing transmission link with rapid project completion and minimal transmission disruption.

Our offering

Hitachi Dolwin5 , Emden, Germany
Foto Jonas Bilberg

HVDC Light®

HVDC Light®

Uses VSC technology for long-distance underground and underwater power transmission, featuring “invisible” power lines, neutral electromagnetic fields, oil-free cables and compact converter stations.

Learn more

HVDC Classic

HVDC Classic

Is used to transmit power over long distances from remote generation, connect grids and link AC systems, especially where the conventional AC methods cannot be used.

Learn more
Multi-terminal HVDC system

HVDC converter station

HVDC converter station

Electricity is converted from AC to DC current, and vice versa, in a converter station. This is done by means of high-power, high-voltage electronic semiconductor valves.

Learn more
HVDC Service

Life-cycle services for HVDC

Life-cycle services for HVDC

Hitachi Energy has long experience in providing maintenance service and delivering upgrades for HVDC links all around the world.

Learn more

IdentiQ™

IdentiQ™

A solution for sustainable, flexible and secure power grids. IdentiQ™ for HVDC uses digital twin technology with state-of-the-art data visualization, to provide clear operational insights in real time.

Learn more
New York City

Hitachi Energy to support major renewable electricity transmission between Canada and New York City

HVDC Light® transmission system will transfer renewable energy for up to 1 million New York homes and help achieve the state’s climate goals
20-09-2022 | 4 min read
Germany’s energy transition system

Hitachi Energy supports huge step in Germany’s energy transition

Our HVDC Light® transmission system will transfer renewable energy for up to 5 million households and help Germany achieve its 2045 carbon neutrality goal.
03-08-2022 | 3 min read

Something caught your eye?

Our sales team will get in touch with you