Scegli la tua regione e lingua

Vai

Menu

Project Engineering Entry Professional

The opportunity

Project Engineering focuses on designing, communicating, and implementing an operational plan for completing an engineering-based project including: Preparing designs, project controls and specifications, schedules, cost estimates, production, transportation, installation, testing and/or commissioning of new infrastructure, facilities, equipment, etc. Monitoring progress and performance against the project plan; taking action to resolve operational problems and minimize delays. Identifying, developing, and gathering the resources necessary to complete the project. May include preparing engineering standards, designs and work specifications; developing project schedules, budgets and forecasts; and selecting materials, equipment, project staff, and external contractors An Entry Professional (P1) applies broad theoretical job knowledge typically obtained through advanced education. May require the following proficiency: Work is closely supervised. Problems faced are not typically difficult or complex. Explains facts, policies and practices related to job area.

How you’ll make an impact:

  • Preparation of LCC schematics for High Voltage Gas Insulated Switchgear (66 kV and above)

  • Preparation of GIS CB / Disconnector / Earthing switch / Fast Acting Earthing switches / CT & VT schematics.

  • Preparation of JB’s for CT, VT, and Density monitors.

  • Preparation of Interlocking table and schematics for various Busbar configurations.

  • Addressing the technical queries raised by the customer during the execution of a project, if required.

  • Interaction with various cross-function teams like Primary, Project Management, and Production, when required.

  • Self-reviewing the documents before submitting them to the Lead Engineer

  • enerating Preliminary BOM by understanding the importance and consequences of releasing it

  • Preparation of Mimic boards inline with SLD and Layout drawings

  • Understanding and preparation of Communication Architecture diagrams

  • Preparation of protection schematics (Trafo, Line, Busbar) when we’ve integrated protection in LCC .

  • Selection of Bay Control Unit and other protection IEDs (Basic level) .

  • Preparation of complete Digital LCC drawings as part of Digital Substation (with NCITs, MU’s, SAM600 modules, etc...) .

  • Preparation of Gas Density monitoring panels using MSM (Modular Switchgear Monitoring).

  • Adhering to applicable codes, practices, QA/QC policies, performance standards, and specifications.

  • Responsible to ensure compliance with applicable external and internal regulations, procedures, and guidelines.

  • Living Hitachi Energy’s core values of safety and integrity, which means taking responsibility for your own actions while caring for your colleagues and the business.

Your Background:

  • Years of experience: 2 – 4 years with B.E / Diploma in Electrical & Electronics Engineering

  • Excellent knowledge of CAD tools (Good to have experience in e3, not mandatory)

  • Very Good knowledge of Protection & Control Systems for T & D .

  • Familiarity with codes and applicable standards like IEC, IEEE, ANSI, etc...

  • Basic knowledge of GIS  Ability to work with multiple discipline projects

  • Ability to work in a team and maintain professionalism.

  • Good communication and interpersonal skills.

    Sede Chennai, Tamil Nadu, India
    Tipo di lavoro Full time
    Esperienza Entry Level
    Funzione lavorativa Engineering & Science
    Contratto Regular
    Data di pubblicazione 2026-03-16
    Numero di riferimento R0121926

    Hitachi Energy

    Hitachi Energy è un leader tecnologico globale nell'elettrificazione, che promuove un futuro energetico sostenibile grazie a tecnologie innovative per le reti elettriche, incentrate sul digitale. Oltre tre miliardi di persone dipendono dalle nostre tecnologie per dare energia alla propria vita quotidiana.

    Con oltre un secolo di esperienza pionieristica nelle tecnologie mission-critical di alta tensione, trasformatori, automazione ed elettronica di potenza, stiamo affrontando la sfida energetica più urgente del nostro tempo: bilanciare la crescente domanda di elettricità con la decarbonizzazione del sistema energetico.

    Con sede in Svizzera e oltre 50.000 persone in 60 paesi, Hitachi Energy genera fatturato per circa 16 miliardi di dollari. Candidati oggi stesso!