Grid-enSure™

Grid-enSure™
Resilience and stability redefined

Overview of Grid-enSure™ power grid solutions, based on power electronics and advanced control systems, enhancing grid resilience, flexibility and supporting grid modernization.

The new challenges for energy players

The world's energy grids are evolving at an unprecedented pace due to changes in the generation mix, load demand, and the broader power ecosystem. Without the right actions and grid solutions, the future more complex power grid will be weaker, less controllable, more decentralized, and less resilient.
Weakness of the grid
The rise in distributed renewable energy sources has decentralized power production. This shift is essential for sustainability but also requires significant adjustments in grid management.
Decentralization of the grid
The decentralization of the grid and the integration of diverse energy sources necessitate sophisticated control systems capable of active demand response.
Lack of resilience and stability of the grid
Technologies like synthetic inertia and fast frequency response enhance grid stability and support resilient power grid operations.

What is Grid-enSure™?

Grid-enSure™ is a fully integrated portfolio that comprises Hitachi Energy’s top end solutions, present and future, based on Power Electronics and Advanced Control Systems.​ Designed to enhance the flexibility, resilience and stability of the grid

Future-proof solutions available today

The Grid-enSure™ portfolio encompasses cutting-edge Static Compensator (STATCOM), High Voltage Direct Current (HVDC), Static Frequency Converter (SFC) and Energy Storage Solutions (ESS) technologies to deliver future-proof functionalities such as voltage support, fast frequency response, synthetic inertia, fault current contribution, and enhanced system strength.

STATCOM

Provides dynamic voltage support and reactive power compensation to enhance grid stability and efficiency.

SFC

Ensures a stable, balanced and controlled frequency conversion of power for various grid applications such as hydro power, rail networks and grid interties, supporting seamless integration of diverse energy sources.

HVDC

Enables high-efficiency, long-distance power transmission, facilitating the integration of renewable energy sources and enhancing grid reliability.

ESS

Digital innovation ecosystem enabling energy management and optimization through battery storage systems, automated and digital capabilities, and delivering grid flexibility services.

What’s unique?

The full verticalization of our systems drive value to our customers across: ​
  • Best state-of-the-art functionalities ​
  • Higher reliability thanks to the optimization of the design, material selection and testing ​
  • Ability to meet the demand thanks to the full control on the supply chain
  • Co-creation of new solutions in partnership with our customers
Semiconductors

Semiconductors are the silent heroes in your daily life. They light up homes, power electric cars, drive electric buses, and advance the world’s energy system to be more sustainable, flexible, and secure. Hitachi Energy’s Semiconductors is a motor driven by people, values and innovation to advance a sustainable energy future for all.

 

Power consulting

Hitachi Energy's Power Consulting advisory services holistically assist customers in identifying grid challenges and recommend customized feasible solutions, combining the know-how on the latest technologies including Power Electronics and control systems, with the mastering of standards and local grid codes.

 

Key benefits to redefine grid resilience and stability

Discover how Grid-enSure delivers the essential elements needed to keep your power grid resilient, stable, and flexible through advanced grid solutions, ensuring reliable power supply and peak performance.
Increasing the reliability of supply
Strengthening the resilience of the grid
Keeping a changing grid under control
Boosting the integration of renewable energy
Increasing power transfer & unlocked capacity

Power Electronics, a cornerstone of grid modernization solutions, is based on the latest semiconductor technology and enables fast, secure conversion and control of energy flows across the power grid ecosystem

High power density

The latest generation of semiconductors can carry +20% more current. This increase in power density enhances operational efficiency, reduces footprint, and improves reliability.

+0%

more current

Boosts the integration of renewable energy

Increases power transfer & unlocks capacity

Higher switching frequency

The higher switching frequency of the semiconductors (x10 – x100) reduces the dampening of harmonics into the grid, thus reducing the need of filters in low power applications (i.e. eMobility).

10x-100x higher switching frequency of the semiconductors

Reduces power losses

Increases reliability 
of supply

Our experts' view

Customer Stories

Part of categoryCustomer Story
TransnetBW enhanced STATCOM, Germany

The TransnetBW Germany project improves power quality for 11 million people by using innovative SVC Light® STATCOM and a 150 MW storage system, significantly reducing CO2 emissions and enhancing grid stability and efficiency.

Part of categoryCustomer Story
Caithness-Moray Shetland 
HVDC Link, UK

The HVDC Links in Scotland project strengthened the power network by integrating renewable energy and linking Shetland to the UK transmission system, using advanced HVDC Light® technology to enhance grid stability and reduce emissions.

Part of categoryCustomer Story
+20% current with same size Semiconductor, Worldwide

The new generation of Hitachi Grid-enSure semiconductors offer a 20% increase in current capacity without increasing the size, improving operational efficiency and power density.

Part of categoryCustomer Story
Waratah Super Battery, Australia

The new Waratah Super Battery near Sydney will enable the nation’s largest city to keep the lights on, while helping Australia meet its renewable energy target of adding 33,000 gigawatt-hours (GWh) each year through 2030.

We are ready. Are you?

Today we can already face the challenges of the future energy system and make it more sustainable, flexible, reliable and secure.