Choose your region and language

Go

Menu

The digital energy transition: Connecting data, systems, and people for a resilient grid

Blog Post | 05.03.2026 | 9 min read | Andy Howell

How Hitachi Energy’s software and collaborations are powering the future of electrification

At a recent Hitachi Energy customer event, a grid manager from a U.S.-based utility proclaimed that wires, poles, and pipes are important, of course, but today data is king.

He emphatically noted that surfacing data from the field and assets is crucial. However, understanding how to quickly and accurately take decisive action based on that data is paramount.

The International Energy Agency reports that “around USD 2.2 trillion (of investments) are going collectively to renewables and electrification.” With this surge of investment comes an unprecedented explosion of data—data that utilities must be able to surface, ingest, and transform into actionable intelligence if they want to stay competitive.

In today’s rapidly accelerating era of electrification, data isn’t just helpful; it’s vital. It underpins reliability, informs real‑time decisions, and ultimately strengthens the resilience of the modern grid.

The digital grid has endless potential

As the demands of electrification, AI, and the broader digital economy continue to grow, the success of the energy transition will hinge on how quickly and effectively we deploy digital intelligence.

For Hitachi Energy’s Enterprise Software Solutions, one truth is unmistakable: Digitalization is essential. As grids become more dynamic, as renewable penetration rises, and as utilities face mounting pressure to respond faster, operate smarter, and plan with greater precision, enterprise software becomes the connective tissue that holds the energy ecosystem together.

This is where energy software plays a defining role. Energy software refers to the digital platforms and applications that collect, analyze, and act on data across the entire energy value chain - from planning, operations and asset management to real-time grid management and energy market participation. It transforms raw grid and asset data into actionable intelligence that improves reliability, efficiency, and resilience.

Hitachi Energy’s enterprise energy software portfolio sits at the center of that transformation. Designed not as isolated tools but as an end‑to‑end system, it breaks down silos and unlocks the full value of data flowing from the grid and across the energy lifecycle - in all directions.

Portfolio built for the entire energy value chain

Hitachi Energy’s digital energy portfolio is built around three major energy software businesses: Grid & Generation Management, Asset & Work Management, and Energy Portfolio Management. Together, these end-to-end energy software solutions enable utilities and other asset-intensive organizations to plan, build, operate, maintain, and commercialize grid and energy systems, forming one continuous flow rather than discrete, disconnected steps across the energy lifecycle.

  • Grid & Generation Management powers the operation and real-time management of the grid itself. It delivers a mission-critical application, Network Manager, that responds to dynamic grid conditions, enabling control across generation, transmission, distribution, and electricity markets.

    ARC Advisory Group recognized Hitachi Energy as the market share leader in Grid Control & Management, Outage Management, and AI Applications, in its Grid Automation Global Market Study 2024-2029 (June 2025).
  • Asset & Work Management focuses on the people and equipment behind the grid: where assets are, their condition, when they need maintenance, and which crews should be deployed to maintain them.

    IDC named Hitachi Energy a Leader in the IDC MarketScape: Worldwide Utilities Asset Performance Management (APM) 2025–2026 Vendor Assessment, noting, “Hitachi Energy can provide a fully integrated APM + enterprise asset management (EAM) + field service management (FSM) suite, which can provide a data-rich asset lifecycle management strategy…."
  • Energy Portfolio Management brings the commercial layer into the fold, ensuring utilities can model prices and energy projects, trade electricity, and optimize the economic value of every electron, energy commodity, and asset. 

What makes this energy software portfolio exceptional is its coherence. Energy-intensive organizations may adopt individual solutions, but greater value emerges when they are connected. This is when planning informs operations, when asset health influences dispatch and future investments, and when commercial decisions reflect real-time grid behavior, energy prices, and power supply.

This unified architecture is not an accident. It responds to an industry in which legacy silos, those between planning, operations, trading, engineering, and field work, are rapidly becoming unworkable. The market pressure, regulatory requirements, and the speed of business are all driving the need for deeper integration. Energy organizations can no longer afford the luxury of slow feedback loops; the lifecycle must move at the pace of the energy transition.

 

Software: The central nervous system that makes the grid intelligent

For decades, Hitachi Energy has been a global leader in hardware including HVDC systems, transformers, switchgear, and other mission-critical components of the grid. Yet even the most advanced hardware is only part of the story. Increasingly, that equipment is becoming intelligent, self-monitoring, and automated.

A future is coming where transformers can diagnose themselves, equipment can signal impending issues, and the grid operates with far fewer manual interventions. This is only possible when hardware and data are connected across the system. And software is the only way to make sense of enormous volumes of data, automate decisions, and ensure that assets perform at their highest potential.

This approach has been forming for 40 years, starting with information and intelligence in early ERP systems and, evolving through decades of control systems, asset databases, and trading platforms. Today, the rise of AI and machine learning is amplifying that foundation exponentially. Algorithms can now analyze what once required teams of experts, compressing time from weeks or months to seconds. The result? Decades of embedded expertise inside the energy ecosystem can be managed and activated in real time.

Breaking down silos to accelerate the energy transition

Modern grids face unprecedented challenges. Demand is rising. Renewable variability is increasing. Decarbonization targets are tightening. And the complex planning processes required to add new infrastructure, such as large battery energy storage systems (BESS) and renewable generation, are still far too slow.

In some cases, planning and permitting can take years. The industry can no longer afford those timelines. To speed this cycle, utilities must be able to run hundreds of thousands of scenarios, share data across teams seamlessly, and shorten planning and implementation horizons from multi-year processes to timelines measured in months. This requires breaking down internal silos and adopting digital tools that allow planning and operations to be tightly linked.

It also requires trust in data - data that is accurate, connected, and accessible to those who need it. Only then can organizations run faster contingency analyses, explore alternative configurations, and make high-confidence decisions that accelerate the clean energy transition.

In this context, digitalization is a key driver in meeting electrification goals, not just part of an efficiency play.

Innovation through collaboration

Hitachi Energy recognizes that no single organization - no matter how experienced - can transform the global energy system alone. That’s why collaboration sits at the heart of its digital strategy.

The future in motion looks like this:

  1.  A unified national grid platform in Japan
    Japan is on a mission to digitally unify the country’s grid and 10 transmission companies—harmonizing load balancing, frequency control, and market operations across regions that historically operated separately. Hitachi Energy is delivering what is expected to become the largest energy management system (EMS) in the world, enabling end-to-end visibility and optimization across an extraordinarily complex network.
  2. Cloud-based grid control for renewable generation operators
    In another example, a U.S. independent power producer, Conduit Power, adopted a fully cloud-based control system, eliminating the need for a traditional physical control room. When severe storms hit Texas, operators were able to run the system remotely from their homes, keeping renewable generation online throughout the event. This represents a fundamental shift: the grid is no longer bound by geography, physical infrastructure, or legacy operational models.
  3. AI‑accelerated interconnection planning for a U.S. regional transmission operator 
    Southwest Power Pool (SPP) is partnering with Hitachi to deploy an AI‑based solution that helps significantly speed generator interconnection studies by up to 80%, enabling faster, higher‑quality decisions as the region works to integrate growing energy resources, including renewables. As regional electricity demand rises, driven by data centers, manufacturing, and electrification, the solution helps SPP address capacity shortages, improve grid reliability, and respond more effectively during emergencies.

These examples illustrate a broader movement, one in which co-creation with customers is shaping the future of energy innovation. Real-world deployments provide the proving ground where new ideas become reliable, scalable solutions.

A connected ecosystem for the future of electrification

Beyond these customer deployments, Hitachi Energy collaborates with leading technology organizations. Innovators including AWS, Google, Microsoft, NVIDIA, are accelerating breakthroughs in AI, cloud, forecasting, and advanced analytics. These partnerships expand capabilities, enhance situational awareness, reduce low‑value administrative tasks, and unlock new layers of data-driven value, importantly accelerating the speed and accuracy of work.

Together, these collaborators and customers form a growing ecosystem: a network of innovators building digital innovations that are connecting all of us to what’s next…a future-ready energy operation.

The message is clear. In the electricity era, connection is power. And as electrification reshapes economies, industries, and communities, the organizations that thrive will be those who harness the full potential of connected data, connected systems, and connected people.

Hitachi Energy is committed to leading that journey.

This season of the Power Pulse podcast focuses on grid automation and digital capabilities, where we will explore many of the topics addressed here and others related to the age of electrification.

Catch the latest Power Pulse podcast episode with Andy Howell, Global Head of Enterprise Software Solutions, now.

Join us: Apple, Spotify, Amazon

FAQ

Energy software refers to the digital applications and platforms that collect, analyze, and act on data across the energy value chain—from grid operations and asset management to market participation. It is essential because it helps utilities improve reliability, make faster decisions, enhance efficiency, and build a more resilient grid.

Digitalization enables energy organizations to ingest high‑volume data, automate complex tasks, model scenarios, and operate the grid with greater accuracy and speed. By connecting planning, operations, and market activities, digital tools accelerate renewable integration, support electrification, and help utilities meet decarbonization goals.

Hitachi Energy’s enterprise energy software is designed as an integrated, end‑to‑end system that unifies grid management, asset and work management, and energy portfolio management. This connected architecture breaks down operational silos, improves data visibility, and ensures utilities can plan, operate, maintain, and optimize their systems as one continuous digital lifecycle.


Andy Howell
Global Head of Enterprise Software Solutions Product Group

Andy leads Enterprise Software Solutions at Hitachi Energy, driving innovation in SaaS, AI, and advanced software for the energy sector. With over 30 years of experience in the hydrocarbon processing industry, he has a deep understanding of the challenges and opportunities that our clients face. His mission is to leverage cutting-edge technology and robust methodologies to create personalized, sustainable solutions that enhance efficiency, safety, and profitability.