ABB wins framework contract worth over $100 million to strengthen Italy’s power grid

Features | Zurich, Switzerland | 12.12.2019 | 2 min read

ABB Power Grids contracted by Terna to provide gas-insulated switchgear as a result of a European tender

ABB has signed a four-year framework contract worth more than $100 million with Italy’s transmission system operator (TSO), Terna. The TSO is responsible for securing and dispatching electricity throughout the country.

Terna will utilize advanced technology from ABB to strengthen Italy’s grid. The contract includes the supply of ABB’s gas-insulated switchgear (GIS), a solution that enables a significant reduction of equipment footprint to just one tenth of the space occupied by air-insulated switchgear substations.

ABB’s GIS solutions enable substations to be built within cities, located within buildings, underground and on rooftops, to supply safe and reliable power. GIS is a compact and reliable solution that enables safe operations in confined spaces.

Image 1

ABB pioneered GIS technology over 50 years ago and continues to drive innovations in this space. As a market and technology leader in high-voltage GIS technology, ABB offers ratings and applications from 72.5kV to 1,200kV and has a global installed base of more than 35,000 bays. ABB’s latest offering includes eco-efficient and digital capabilities.

ABB (ABBN: SIX Swiss Ex) is a technology leader that is driving the digital transformation of industries. With a history of innovation spanning more than 130 years, ABB has four customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by the ABB Ability digital plat-form. ABB’s Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 147,000 employees. www.abb.com

Downloads

Contacts

Photo of
Media Relations

Hitachi Energy

全部新闻