地域と言語を選択してください

メニュー

44057

The Gotland HVDC link

The world's first commercial HVDC transmission system, the Gotland HVDC link built in 1954, has over time been replaced with a 260 MW bipole transmission system.

The 20 MW, 100 kV Gotland 1 HVDC link from 1954 was the first commercial HVDC transmission in the world. As the world’s first commercial HVDC link, the Gotland link was awarded a prestigious IEEE award, adding Gotland 1 to the IEEE Milestones program, which honors significant technical achievements across electrical engineering.

The converter valves taken into operation in 1954 were mercury-arc valves. In 1970, the stations were supplemented with thyristor valves which were connected in series with the mercury-arc valves. The voltage was raised to 150 kV and the transmission capacity to 30 MW.

It was the first time thyristor valves were used in a commercial HVDC transmission in the world. Read more about Gotland 1 in: The early HVDC development

Gotland 2 and 3

In 1983, a new cable was laid between the inverter station near Västervik on Sweden's west coast and Ygne station on Gotland. Gotland 2's rated voltage was 150 kV and transmission capacity 130 MW and the converters were built up of thyristor valves. Gotland 2 and Gotland 1 operated independently and together met Gotland's power needs. Fossil fuel generation on the island was shut down and used only for reserve generation.

Increasing demand and concern about supply safety led to a decision in 1985 to build another HVDC link to Gotland, the Gotland 3, which usually works with Gotland 2 to form a bipolar link but can also work independently. The total transmission capacity is 260 MW (max. 320 MW).

The original cable and terminal equipment for Gotland 1 were taken out of service and dismantled in 1986 when Gotland 3 was built. The owner of the link is Vattenfall.

Upgrade to enable more renewable energy integration and boost reliability

In 2017 Hitachi Energy was entrusted to carry out another upgrade to enable more renewable energy integration and boost grid reliability on the island. As a key element of the upgrade Hitachi Energy will install its state-of-the-art MACH control and protection system, the brain of an HVDC link. 

Hitachi Energy’s MACH control system offers unmatched calculation capacity and a high degree of integration capability to handle control and protection functions, designed to run around the clock for 30 years or more. It also incorporates advanced fault registration and remote control functions. The cooling system will also be upgraded as part of the project. The upgrades replace aging equipment and will help improve security of power supply to the island. The addition of a modern operator interface will also help extend the lifetime of the link in addition to providing improved availability and functionality.

Main data
Commissioning year: Upgrade: 2018
Pole 3: 1987
Pole 2: 1983
Power rating: 260 MW
No. of poles: 2
AC voltage: 130 kV (Västervik), 70 kV (Ygne)
DC voltage: ±150 kV
Length of DC submarine cables: 2 x 96 km
Length of DC overhead line: 7 km
Main reason for choosing HVDC: Length of sea crossing
Application: Connecting remote loads