地域と言語を選択してください

メニュー

Energy data analytics: finding value others miss

Blog Post | 11.11.2026 | 5 min read | Bret Toplyn

How connected planning, forecasting and operations help energy organizations make better investments and manage risk

The energy industry's competitive advantage will not come from infrastructure alone. It will come from using data to make better decisions about where to invest, how to operate and how to manage risk—and to recognize opportunities that conventional approaches can overlook.

Michael Lewis's Moneyball, a book later adapted into a film, tells the story of a U.S. baseball team using data to identify undervalued players and compete on a limited budget. Its central lesson extends beyond baseball statistics: better decisions come from using data to identify value that conventional methods miss. The modern grid presents a similar challenge: understanding where infrastructure can create the most value as energy demand, supply and market conditions change.

Data center growth, electrification, battery storage, and renewable integration are reshaping how energy infrastructure is planned, built, and operated.

For utilities, developers, independent power producers, large energy consumers, and investors, the challenge is how to navigate that change alongside supply chain pressures and geopolitical uncertainty, without compromising safety, reliability, or economic performance.

Plan for uncertainty, not a single future

Historical trends still matter, but they are no longer enough to guide long-term infrastructure decisions. Planners must account for concentrated clusters of large loads, variable generation, and batteries that can serve multiple market needs.

Policy uncertainty, commodity price volatility, and extreme weather add further complexity. A developer evaluating a battery project or hyperscale data center may need to assess thousands of possible outcomes.

The investment question is no longer simply, "What will happen?" It is, "What could happen, and which investment performs best across those outcomes?"

Find value beyond the obvious investment

The relevant lesson from Moneyball is to look beyond familiar measures of value and test investment assumptions against the data. In energy markets, that means combining market indicators with electricity demand, weather, transmission, operational and financial data to understand where an asset can create the most value—not simply where it can be built.

What appears to be a simple decision, such as where to place a battery or connect a large load, can require:

  • Production cost simulations
  • Transmission contingency studies
  • Congestion analysis
  • Power flow modeling
  • Capacity adequacy assessments
  • Market price forecasts
  • Renewable generation forecasts
  • Interconnection analysis
  • Financial risk assessments

The objective goes beyond finding a point of connection. It is to understand where an asset can deliver long-term value while maintaining system reliability. The implications can extend 25 years or more.

Advanced planning analytics help test those assumptions by showing how grid constraints and market conditions affect an investment's potential value.

Data and simulation have long supported energy investment decisions. Today’s data volumes and range of scenarios make them essential for answering questions such as:

  • Which transmission upgrades create the highest economic value?
  • Where can batteries provide the greatest congestion relief?
  • Which regions offer the strongest future market revenues?
  • How do large loads impact system economics?
  • Which investments remain resilient across multiple scenarios?
  • How do active positions evolve with ongoing operations?

The highest-value investment is not always the most obvious one.

Testing these possibilities against grid and market data helps reveal opportunities that a single forecast or a familiar investment approach could overlook.

Connect investment decisions to commercial reality

A strong investment case is only the beginning. A project's success also depends on how the asset operates, participates in markets, and manages ongoing risk.

For a battery, generator, transmission asset, or large-load connection, commercialization connects planning assumptions to operational and financial decisions.

Once an asset enters operation, every hour becomes a decision.

The questions shift from what, where, and when to build to:

  • How exposed are we to price volatility?
  • What risks exist with counterparties, credit, or liquidity in the market?
  • How should we hedge risk?
  • How can we optimize revenues and identify new opportunities?

The same data-driven approach must continue after the investment decision. Connecting planning data with updated market prices, forecasts and operational information helps organizations reassess an asset's value and manage risk as conditions change.

Turn battery flexibility into value

Battery energy storage systems (BESS) are a prime example of why connected decisions matter.

Their value depends on when they charge and discharge and how they support the grid. Opportunities include day-ahead markets that trade electricity for delivery the next day, reducing real-time peak-demand periods, and providing ancillary services that help keep the grid stable.

Batteries can also relieve congestion that might otherwise require long-term transmission investments. Turning that flexibility into value requires connected data, forecasting, optimization, and energy trading and risk management (ETRM).

Data provides the foundation for evaluating those opportunities. Aligning grid and market information from different sources, recorded at different time intervals and with different identifiers, creates a trusted basis for decisions.

Forecasting must go beyond a single accurate prediction, enabling rapid testing across possible futures so organizations can assess strategies and adapt.

Optimization turns those insights into operating decisions across time intervals and scenarios. Trusted, reproducible methods help operators and traders defend their choices.

Manage the financial consequences of operational choices

An optimized operating strategy must also account for commercial exposure. ETRM brings that perspective into the decision.

It records energy transactions, positions, contracts, settlements, and risk. Combined with market data, forecasts, and optimization results, this information supports valuation, exposure monitoring, trading strategies, and compliance management.

As volatility, renewable penetration, battery participation, and large-load demand grow, this visibility helps organizations translate planning and optimization into disciplined commercial execution.

Moneyball for the modern grid

The next generation of energy leaders will connect planning, forecasting, optimization, operations, and commercialization within a shared decision-making framework.

The lesson from Moneyball is not to collect more statistics for their own sake. It is to use evidence to challenge familiar assumptions about value and make better decisions.

For energy organizations, that means connecting grid, weather, demand, market and financial data—from deciding where to invest to determining how an asset operates and participates in energy markets. This shared evidence base helps reveal value, manage risk and support reliability as conditions change.

Infrastructure remains essential. Better decisions are what turn it into a lasting advantage.


Bret Toplyn
Director of Product Management, Energy Analytics

Bret Toplyn has nearly 15 years of experience driving analytical software solutions across the global energy sector. He has a proven track record of orchestrating transformative product strategies that fuel growth and adaptability in an ever evolving market.

He specializes in tackling complex energy challenges and delivering innovative, client focused product solutions. Deeply committed to optimizing user experience while leveraging analytics, his expertise lies in aligning product roadmaps with shifting market demands and regulatory landscapes, helping clients maintain a competitive edge in an increasingly dynamic energy marketplace.