Välj din region och ditt språk

OK

Meny

First natural ester power transformer successfully passed the technical appraisal of new products in China for Hitachi Energy

The transformers contribute to decarbonization, enhanced safety for people, protection of ecosystems and responsible use of resources across the transformer’s life cycle.

In November 2022, the SWZ13-63000/110 natural ester power transformer produced by Hitachi Energy Zhongshan Transformers Factory (CNZTC) successfully passed the technical appraisal of new products by Guangdong Machinery Industry Association. The appraisal committee recognized this transformer reached the international advanced level of similar products. 

This also means that CNZTC has obtained the bidding qualification for the natural ester power transformer project of China Southern Grid. This product is the world's first EconiQ™ power transformer for Hitachi Energy. The transformer was successfully put into operation in China’s first "zero carbon" substation demonstration project of the State Grid Corporation of China (SGCC)-Gaoxiang (Qingshu) substation in Wuxi, Jiangsu Province, in February 2022.

SWZ13-63000/110 natural ester power transformer is a new type of environmental-friendly product, which was developed based on the goal of the whole society to achieve carbon peak and carbon neutralization as soon as possible. It is the company’s portfolio of solutions that are proven to deliver exceptional environmental performance resulting in significant reductions in carbon footprint. the transformers are optimized based on the specific sustainability requirements of our customers and Hitachi Energy’s technology domain expertise, using environmental Life Cycle Analysis methodology.

The transformers contribute to decarbonization, enhanced safety for people, protection of ecosystems, and responsible use of resources across the transformer’s life cycle. The transformers are also manufactured using fossil-free electricity at Hitachi Energy facilities, further contributing to the overall reduction of their carbon footprint.

Main data
Customer: State Grid Corporation of China (SGCC)
Product: Power Transformers
Power Rating: 63 MVA, 110/21 kV
Location: Wuxi, Jiangsu, China
Delivery: 2021 December
Technology: Natural ester