Välj din region och ditt språk

OK

Meny

Features 19-09-2019

2 min read

South Korean port to slash passenger vessel emissions with ABB shore power

ABB will install Port of Incheon’s first shore-to-ship power solution, enabling passenger vessels to cut emissions, noise and vibrations at berth

ABB has secured the contract covering South Korea’s commitment to sustainable shore-to-ship power, after a pilot scheme for passenger ships to plug into the local grid received the go ahead from Incheon Port Authority (IPA).

“As the first agreement covering shore-to-ship power in South Korea, this is a truly significant breakthrough for ABB,” said Juha Koskela, Managing Director, ABB Marine & Ports. “We are honored to be selected by IPA to support their efforts in reducing greenhouse gas emissions from ships, as well as moving towards increasingly sustainable port operations.”

In addition to a new USD160 million ferry terminal opened in April 2019, Port of Incheon inaugurated South Korea’s largest cruise terminal in June this year. Given its metropolitan location and IPA’s ambitions to develop its ‘Golden Harbor’ vision for Incheon as a new tourism hub for the Northeast Asia, environmental credentials rank highly in port priorities.

ABB’s full scope of delivery includes the installation of an onshore power connection at the Incheon passenger terminal consisting of an enclosure featuring a 2000 kVA capacity Static Frequency Convertor with 50/60HZ output, a transformer, a Neutral Grounding Registor Unit and an outdoor enclosure.

ABB’s shore-to-ship power technology is proven from the performance and reliability point of view, but also in terms of optimizing the cost of electricity. It has already been integrated by over 50 ports around the world into strategies that reduce emissions overall and incentivize clean shipping.

An increasing number of ports around the world offer shore power for ferries, as well as other passenger vessel types. There is a clear interest to lower pollution in ports, and one way of doing that is to install shore power and have a clean grid feeding to it.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader with a comprehensive offering for digital industries. With a history of innovation spanning more than 130 years, ABB is today a leader in digital industries with four customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by its common ABB Ability digital platform. ABB’s market‑leading Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 147,000 employees.

Contact Us

Media Relations
+41 43 317 71 11